Cancel
Showing results for 
Search instead for 
Did you mean: 

Why is my Line not being displayed?

Genius
Genius

I need to create a large number of unassociated lines in NX.  The below code runs without problem but the lines are never displayed.

 

It feels like I'm missing some minor, trival thing.  Any ideas?

 

	NXOpen::Session *theSession = NXOpen::Session::GetSession();
	NXOpen::Part *workPart(theSession->Parts()->Work());
	NXOpen::Part *displayPart(theSession->Parts()->Display());

	Vector3d direction = Vector3d(end.X - start.X, end.Y - start.Y, end.Z - start.Z);
	double length = sqrt(direction.X*direction.X + direction.Y*direction.Y + direction.Z*direction.Z);
	NXOpen::LineCollection* lines = workPart->Lines();
	NXOpen::CurveCollection * curveColection = workPart->Curves();
	NXOpen::Point* startPnt = workPart->Points()->CreatePoint(start);
	NXOpen::Point* endPnt = workPart->Points()->CreatePoint(end);
	NXOpen::Line* line =curveColection->CreateLine(startPnt, endPnt);

	line->RedisplayObject();

If I journal line creation it calls CreateAssociativeLineBuilder. My assumption is that that would be slower than that what I did above but at least it works.

 

Mark

 

5 REPLIES

Re: Why is my Line not being displayed?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

The line that you have created is a "SmartObject". You will need to use the SetVisibility method to make it visible (it is created as invisible by default).

 

Is your intention to make a 'dumb' curve? If so, you will want to use the RemoveParameters method after line creation. If you do not, you will end up with a line that is neither a dumb curve nor is it an associative curve feature. In your case, the line will be associative to the points; but the user will have no way of editing the resulting line.

 

A few links below for more info:

http://nxjournaling.com/content/creating-lines-part-1

 

http://nxjournaling.com/content/creating-lines-part-2

Re: Why is my Line not being displayed?

Siemens Phenom Siemens Phenom
Siemens Phenom

 

As is often the case in NX, there may be more than one possible solution.

 

If you really just need "dumb" curves, try UF_CURVE_create_line().  The created line will not be invisible, and you will not have to add it to the display.

Re: Why is my Line not being displayed?

Genius
Genius

 

Sigh... it never occured to me it would be off by default. The following did the trick.

 

line->SetVisibility(NXOpen::SmartObject::VisibilityOption::VisibilityOptionVisible);

 

Thanks!

Re: Why is my Line not being displayed?

Genius
Genius

Steve, that worked too with less code. Nothing like the old ways Smiley Tongue

Re: Why is my Line not being displayed?

Pioneer
Pioneer

hi Mark! Did you generate these lines using C++ ? I am curious to know as I am trying to generate curves (in form of the curve points connected via lines) using C++ programming and executing it in NX (in form of .dll).