Cancel
Showing results for 
Search instead for 
Did you mean: 

Win 8 desktop icon change for NX

Gears Phenom Gears Phenom
Gears Phenom

I'm testing a new workstation, and Windows 8, for use with NX9.  We use the NXCustom setup that Rob Cohon developed, so all the custom NX changes, and start up .bat files are on the server, and only the OOTB install is on the local machine.  I'm trying to get the desktop icons for the shortcuts to the .bat files, to use the NX.ico icon file, but they are refusing.  Is there something different I have to do on Wndows 8?  See attached.

 

Thanks,

 Dave

IconWontChange.jpg

-Dave
NX 11 | Teamcenter 11 | Windows 8.1
4 REPLIES

Re: Win 8 desktop icon change for NX

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

How about using the icon from %UGII_ROOT_DIR%\ugraf.exe?

 

If you use the above path with the environment variable, you should not need to change the icon for an upgrade, since the environment variable is used instead of the expanded path.

 

Another option is to extract the icon contained in ugraf.exe, since it should have all the sizes Windows needs.

You could use IcoFX v1.6 or Paint.NET with the icon plug-in to extract the icon with all its sizes.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.1, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: Win 8 desktop icon change for NX

Gears Phenom Gears Phenom
Gears Phenom

%UGII_ROOT_DIR%\nx.ico

 

That worked, it must not like the network location.

-Dave
NX 11 | Teamcenter 11 | Windows 8.1

Re: Win 8 desktop icon change for NX

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I think UNC paths are not supported, but mapped drives surly are.

 

I would still try to reduce network load and use local resource as much as possible.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.1, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: Win 8 desktop icon change for NX

Gears Phenom Gears Phenom
Gears Phenom

Agreed, since we are not using a mapped drive, the local icon is a better idea.

-Dave
NX 11 | Teamcenter 11 | Windows 8.1