Cancel
Showing results for 
Search instead for 
Did you mean: 

Working with NXObject.AttributeType.Real

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

Hello everyone!

 

How do I work with NXObject.AttributeType.Real? I understand that I need to assign Unit as well - but I can't understand how! I intend to add an attribute to the part that will hold the length mm value. Can you please help?

6 REPLIES

Re: Working with NXObject.AttributeType.Real

Esteemed Contributor
Esteemed Contributor

Did you try recording a journal?

 

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP5 + patch/TC11.2
I'd rather be e-steemed than e-diseaseled


Re: Working with NXObject.AttributeType.Real

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

Yes, I did. Journal is using AttributePropertiesBuilder what is not very useful for me in my current situation. I already have few attributes being assigned via NXObject.AttributeInformation and I would like to use this route as well because I do not want to rewrite - if it is possible.

 

I basically made it work, but value is assigned as unitless - and I need mm.

Re: Working with NXObject.AttributeType.Real

Honored Contributor
Honored Contributor

Did you try supplying the unit object to the "unit" field of the attribute structure?

Re: Working with NXObject.AttributeType.Real

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

I don't know how do to this. I found no examples and could not obtain answer from documentation.

Re: Working with NXObject.AttributeType.Real

Honored Contributor
Honored Contributor

This article may be of help.

Re: Working with NXObject.AttributeType.Real

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

Thank you! I will have a look.