Cancel
Showing results for 
Search instead for 
Did you mean: 

bct raster viewer in NX9

Experimenter
Experimenter

I am trying to use BCT Raster Viewer in NX9, but it won't load properly. It says there is a something missing from the .dll file. I use the same viewer in NX6 and 7.5 without any issues. I did try the 64 bit version of the viewer as well with the same result. To be fair 7.5 is the last version listed when installing the viewer, but BCT is supposed to be partners with Siemens.

2 REPLIES

Re: bct raster viewer in NX9

Esteemed Contributor
Esteemed Contributor

You probably need a newer version of the raster viewer (assuming BCT still supports it).

Contact them at http://www.bct-technology.com/

 

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP5 + patch/TC11.2
I'd rather be e-steemed than e-diseaseled


Re: bct raster viewer in NX9

Experimenter
Experimenter

Been there done that.