Cancel
Showing results for 
Search instead for 
Did you mean: 

custom license

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

hi guys ,,, do we can make custom package license from existing license

 

 

let say i wanna make package like this 

PACKAGE ABC ugslmd 31.0 COMPONENTS="MFG_assemblies MFG_cam_base \
                ABC_cavity_milling MFG_drafting MFG_dxf_to_ug MFG_dxfdwg \
                ABC_features_modeling MFG_fix_axis_surf_mill MFG_flow_cut \
                ck=195 SIGN="XXX JKLO 135F B929 102E SSS SSSS A835 6AC6 A993 \
                5555 SSSS SSSS A51C E20E 08C8 FAB0 JJJJ SSSS 2C5F 7210 SSSS \
                6666 B230 UUUU 32D7 5B83 043A 3240 5429"

 

is it can do ?

 

 

7 REPLIES

Re: custom license

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

That is up to you and your Siemens (or VAR) sales rep.

Although I would guess if you only have a couple licenses, probably not.  If you have 2000 licenses, probably yes.  I don't know at what point Siemens is receptive to doing this.

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: custom license

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

thanks for answering this ken, so i take conclusion that action is can doing by our self right ?,  "I don't know at what point Siemens is receptive to doing this" is it mean this do not allow by siemens or what ?, would you give me referrence about tutorial to custom this, i need that, there is need from my customer to do this.

 

Thanks you

Re: custom license

Only Siemens can generate the license file.

What are you trying to do? We offer several license bundles today - what do you need that is different?

Mark Rief
Retired Siemens
Highlighted

Re: custom license

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

Hi Mark

 

i just want to custom existing license 

for example like below

before:

PACKAGE UG12500G ugslmd 31.0 COMPONENTS="UG12500G_assemblies \
UG12500G_features_modeling UG12500G_gateway \
UG12500G_grip_execute UG12500G_id_ext_fem_beam UG12500G_iges \
UG12500G_nx_ansys_export UG12500G_nx_freeform_1 \
UG12500G_nx_freeform_2 UG12500G_nx_ftk UG12500G_nx_masterfem \
UG12500G_nx_material_system UG12500G_nx_nastran_export \
UG12500G_pcf_package_file UG12500G_pstudio_cons \
UG12500G_pv_ugdatagenerator UG12500G_sla_3d_systems


i wanna being split like this

 

after:
PACKAGE UG12500G ugslmd 31.0 COMPONENTS="UG12500G_assemblies \
UG12500G_features_modeling UG12500G_gateway \
UG12500G_grip_execute UG12500G_id_ext_fem_beam UG12500G_iges \


PACKAGE XYZ ugslmd 31.0 COMPONENTS="UG12500G_assemblies \
XYZ_nx_ansys_export UG12500G_nx_freeform_1 \
XYZ_nx_freeform_2 UG12500G_nx_ftk UG12500G_nx_masterfem \
XYZ_nx_material_system UG12500G_nx_nastran_export \
XYZ_pcf_package_file UG12500G_pstudio_cons \
XYZ_pv_ugdatagenerator UG12500G_sla_3d_systems

 

 

my customer ask for custom like above

Re: custom license

Please talk to your Siemens account representative about available license bundles and add-ons. 

Mark Rief
Retired Siemens

Re: custom license

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
When you say "my customer ask for custom like above" - are you a VAR? (reseller of NX)? If so, you really need to talk with someone directly in the Siemens PLMS who is your contact for issues like this.
Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: custom license

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

yes i am VAR, oke thank you Ken i will talk to siemens representative in area.