Cancel
Showing results for 
Search instead for 
Did you mean: 

flip the UF_UDOBJ_query_class_id_t flag for a UDO class in a part file

Valued Contributor
Valued Contributor

Is there a simple way to flip the UF_UDOBJ_query_class_id_t flag of a class in a part file?  I can find the text string of the UDO class's name in the file, but using a hex editor to flip nearby 1 values to 2 didn't do the trick.

2 REPLIES

Re: flip the UF_UDOBJ_query_class_id_t flag for a UDO class in a part file

Siemens Phenom Siemens Phenom
Siemens Phenom

 

I think the design intent is that the flag is set when a UDO is created, and cannot be changed.

Re: flip the UF_UDOBJ_query_class_id_t flag for a UDO class in a part file

Valued Contributor
Valued Contributor

I gathered that much. Smiley Happy  Of course, I'm hoping it is just an independent flag, and that no other part of the state of one of these things depends upon that flag.