Cancel
Showing results for 
Search instead for 
Did you mean: 

journal for print screen with user input

Experimenter
Experimenter

please any one know journal for print screen , and then user can input the name for that file and then user can select path for that file 

2 REPLIES

Re: journal for print screen with user input

Siemens Phenom Siemens Phenom
Siemens Phenom

You don't really need a journal for this as it is a built in command. Use File, Export, [PNG, JPEG, GIF, TIFF, BMP].

 

You can put the UI into customize mode and drag the command (hold down <Ctrl> to make a copy) to add it to any ribbon bar or menu that you want.

 

The dialog includes a browse button for selecting the file name and a toggle to use a white background.

Re: journal for print screen with user input

Gears Legend Gears Legend
Gears Legend

Have a look at C:\Program Files\Siemens\NX 11.0\UGOPEN\SampleNXOpenApplications\.NET\SnagImage

Patrick Delisse
KMWE - DutchAero
NX 12.0, TC 11.2, CAMPOST V22, Vericut 8.1, TDM 4.8
C#, VB, .NET