Cancel
Showing results for 
Search instead for 
Did you mean: 

license NX10

Solution Partner Builder Solution Partner Builder
Solution Partner Builder
Dear all
I have a question about license file . Can I use license NX10 to run NX4 ?

Thank you
2 REPLIES

Re: license NX10

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

No, starting with NX 5 a new license file format is used.

 

For NX 4 and below you need to use the NX 4 license server.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.1, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: license NX10

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

To be specific:

NX5 & newer use the vendor daemon "ugslmd" (note the "s")

NX4 & older (back to UGII v14 or so) use the vendor dameon "uglmd" (without the "s")

 

You can run *one* of each daemon on the same computer (i.e. one uglmd and one ugslmd)

 

(in case you're interested, UGIIv13 & earlier used ACS, not flexlm/flexnet/whatever they're calling it now)

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled