Cancel
Showing results for 
Search instead for 
Did you mean: 

making JT model

Pioneer
Pioneer

I have assemblies in NX (465 total). I want to convert them in JT. I also have made a macro tool, but evertime it requires me to click the button. I am looking for something basicallly a program that would conduct this process in the background instead of me opening the assemblies and getting it done each time. Is there any way I can create a program for the 465 assemblies.

 

 

Thanks in advance

 

Pooja 

6 REPLIES

Re: making JT model

Ganesh_Kadole 2nd Gear
2nd Gear

Native NX or Managed NX?

Ganesh Kadole, QA Analyst (PLM), SQS
Testing: NX 11 | NX 12 | TCIN
TC 11.2 | TC Vis 11.3 | AWC 3.2

Re: making JT model

Pioneer
Pioneer

Native NX

Teamcentre 11 and NX 10

Re: making JT model

Ganesh_Kadole 2nd Gear
2nd Gear

Have a look at this topic

https://community.plm.automation.siemens.com/t5/NX-Design-Forum/Is-there-a-Way-to-Batch-Export-JT-or...

 

Ganesh Kadole, QA Analyst (PLM), SQS
Testing: NX 11 | NX 12 | TCIN
TC 11.2 | TC Vis 11.3 | AWC 3.2

Re: making JT model

Ganesh_Kadole 2nd Gear
2nd Gear

Hi @pghatge,

 

You can create a shortcut of 'run_ugtopv.bat' and use it with windows explorer send to option as mentioned below.

First create a shortcut of file 'run_ugtopv.bat' located at path "C:\Program Files\Siemens\NX 10.0\PVTRANS" to the desktop.

In windows explorer address bar type 'shell:sendto', enter. It will open 'SendTo' folder of windows of the current user.

Cut/paste the shortcut here. Rename and change icon of shortcut as you needed. In my case I renamed it as Convert to JT and used NX icon.

 

jtfile.PNG

 

In the folder where assembly files are present, select the assembly root file > Right Click > Convert to JT. Or create a text file and mention the full path of all the root assembly part files including the .prt extension. Select text file > Right Click > Convert to JT, it will create the JT for all the assembly part files depending upon the preferences set to the 'tessUG.config' file.

 

jtfile.PNG1.PNG

  

jtfile1.PNG

 

Ganesh Kadole, QA Analyst (PLM), SQS
Testing: NX 11 | NX 12 | TCIN
TC 11.2 | TC Vis 11.3 | AWC 3.2

Re: making JT model

Pioneer
Pioneer

Hello Ganesh

 

Thanks a lot for your reply. I am going to try this method and get back to you. I seriously have a deadline for the project am working on. Or ill will have to build a program in VB which would take me ages, since I have very little knowledge of programing. 

 

Again thanks for your suggesstion

 

Regards 

Pooja

Re: making JT model

Pioneer
Pioneer

Can you share me your jt.txt file. I am trying to save the location but it wont work out for me.