Cancel
Showing results for 
Search instead for 
Did you mean: 

pass values with "<>" from excel

Valued Contributor
Valued Contributor

hello all,

 

in the moldwizard cutomization, imagine that i have  a "COLUM A" and a example value of it is <VALUEA>

 

when inserting, NX assumes that im transfering a expression because of the <> , is there a way to bypass this (and yes i want the <> )?

W10 - NX 9 - 10 - 11 - 12 - MW - Journaling || vegetagaru @ engtips
4 REPLIES

Re: pass values with "<>" from excel

Creator
Creator

Hi, I don't think that you can bypass those <>, they are made to create link in the expression in the excel sheet.

Re: pass values with "<>" from excel

Valued Contributor
Valued Contributor

i was wondering if someone have values with those "<>" because if they have, they have to countor that in some way xD

W10 - NX 9 - 10 - 11 - 12 - MW - Journaling || vegetagaru @ engtips
Highlighted

Re: pass values with "<>" from excel

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

In NX, the < and > characters have special significance when used in a note. If you want the literal characters to show up in the note, they need to be preceded with a $ character; so $<some note$> would show up as <some note>.

 

I'm not a moldwizard user, so I don't know if the same applies there.

Re: pass values with "<>" from excel

Valued Contributor
Valued Contributor

cowski the saviour Smiley Very Happy thank you

W10 - NX 9 - 10 - 11 - 12 - MW - Journaling || vegetagaru @ engtips