Cancel
Showing results for 
Search instead for 
Did you mean: 

point annotation

Assume that you have point as udo and annotations should be like attached image...

 

is it possible through code??...if yes can you please share a small prototype of above use case..

2 REPLIES 2

Re: point annotation

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

PMI on model?

Or on a drawing in drafting?

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Highlighted

Re: point annotation

I want to attch pmi to nxObject  in 3D