Cancel
Showing results for 
Search instead for 
Did you mean: 

run exe application in vb.net

Pioneer
Pioneer

Hello,

I've created an exe application in vb.net using NX10 Wizard. Can you plz tell me some suggestive measures as to how we run the exe application  and interact with NX session in VB.Net?

Your help will be appreciated!

 

Thanks,

Juhi.

2 REPLIES

Re: run exe application in vb.net

Siemens Phenom Siemens Phenom
Siemens Phenom

File -> Execute -> NX Open -> Pick your program, then OK.

 

The shortcut for this is Ctrl+U.

 

Note that if you intend for your program to run within an interactive session of NX, you can build it as a shared library - a .DLL.  But when you are using NX Open .Net, you can run either a .DLL or a .EXE this way.

Re: run exe application in vb.net

Creator
Creator

Hello,

One long way to execute nxopen.Net application external is to use remoting.Use remoting example in unigraphics folder.Implement your code in client application.First execute the Server application(Server.dll) using NXStartup.Then execute client in VB. If possible launch NX via using Start method from Process class (System.Diagnostics).

Thanks.