Cancel
Showing results for 
Search instead for 
Did you mean: 

the LW not fast enough in displaying info

Phenom
Phenom

To all

 

I have a small code which does the following

 

theLW.WriteLine("-Creating dictionaries...")
  'create dico1
  'create dico2
theLW.WriteLine("--Done")

theLW.WriteLine("-Processing file...")
  'do something
theLW.WriteLine("-File processed...")

 

I was hoping that the info in the LW is "printed" as the program progresses to let the user know what is happening but all the messages are printed almost in a block. The steps create 'dico1' and create 'dico2' may take a few seconds and yet I do not get the sequence

Message 1 printed

Nothing is happening while the dictionaries are created

Message 2 printed

Does anyone know if there is a way of controlling the LW?

 

Thanks

Regards

Production: NX.CAE 10.0.2.6
Development: VB.NET (amateur level !)
3 REPLIES 3

Re: the LW not fast enough in displaying info

Genius
Genius

Hi!

 

Perhaps you can solve your problem with some simple threading.

You can try to start a new thread which will write "Creating Dictionaries" in the LW

(or MessageBox) and wait for him to stop before you proceed with further commands.

First you need to import

Imports System.Threading

and you need a sub like this:

Sub writeLWStart()

MsgBox("Starting Dico")

End Sub

 

Now you can initiate and start a new thread with

Dim Thread1 As New System.Threading.Thread(AddressOf writeLWStart)

Thread1.Start() ' Starting new thread

Thread1.Join() ' Waiting until the thread is done

MsgBox("End") ' or creating you dicos ..

 

 

You can also terminate your thread manually with an additional sub, if neccessary.

Hope that helps!

 

Bye,

 

Flo

Re: the LW not fast enough in displaying info

Siemens Phenom Siemens Phenom
Siemens Phenom

@selex_ct,

 

Try NXOpen.UF.UFUi.UpdateListingWindow to flush the list window buffer.

 

https://docs.plm.automation.siemens.com/data_services/resources/nx/10/nx_api/en_US/custom/ugopen_doc...

 

Rather than calling this after every theLW.WriteLine, I wrote a wrapper function:

 

    Sub logOutput(ByVal stringList As List(Of String))

        theLw.Open()

        For Each line As String In stringList
            theLw.WriteLine(line)
        Next line

        theUfSession.Ui.UpdateListingWindow()

    End Sub

Re: the LW not fast enough in displaying info

Phenom
Phenom
thanks to both Jimb and FlolScreen for the suggestions. Will have a look at both. in the meatime I have also tried the use of: ufs.Ui.SetPrompt and it could be a way around it. It's just less obvious to the user what his happening
When I process the file I am experimenting with something like
dPercProgress = Math.Round(100*(i/ListofFELabel.Count),1)
ufs.Ui.SetPrompt("% Progress: "& Cstr(dPercProgress))

Thanks
Regards
Production: NX.CAE 10.0.2.6
Development: VB.NET (amateur level !)