Cancel
Showing results for 
Search instead for 
Did you mean: 

toggle disables group

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Hello,

i'm new in programming.

I have created a dialog by using the Block ui styler of NX.

Dialog.PNG

 

Here is a toggle in that enable/disable a other group of settings in this dialog.

How do i need to set the VB script that this is also happening?

 

do i need to place some scripting in this part:

    Public Function update_cb(ByVal block As NXOpen.BlockStyler.UIBlock) As Integer
        Try
       
            If block Is Active_mode Then
            '---- Enter your code here -----
           
            ElseIf block Is Test1 Then
            '---- Enter your code here -----
           
            ElseIf block Is Test2 Then
            '---- Enter your code here -----
           
            End If
       

 

 

Thanks for the tips.

 

 


Ruud van den Brand
Pre-sales NX CAD
cards PLM Solutions
3 REPLIES

Re: toggle disables group

Gears Phenom Gears Phenom
Gears Phenom

if you are asking if this is the place to put some to do something everytime the user clicks on a toggle then yes

Production: NX.CAE 9.0.3.4, NX.CAE 10.0.2.6
Development: VB.NET (amateur level !)

Re: toggle disables group

Siemens Phenom Siemens Phenom
Siemens Phenom

You'll want to add the following line in a couple of places: group.Show = toggle0.Value

 

First, in the update callback, to capture any interactive changes:

 

    Public Function update_cb(ByVal block As NXOpen.BlockStyler.UIBlock) As Integer
        Try
        
            If block Is toggle0 Then
            '---- Enter your code here -----
                group.Show = toggle0.Value
            
            ElseIf block Is toggle01 Then
            '---- Enter your code here -----
            
            ElseIf block Is toggle02 Then
            '---- Enter your code here -----
            
            End If
        
        Catch ex As Exception
        
            '---- Enter your exception handling code here -----
            theUI.NXMessageBox.Show("Block Styler", NXMessageBox.DialogType.Error, ex.ToString)
        End Try
        update_cb = 0
    End Function

 

And also in the dialog shown callback, so that the dialog is loaded in the correct state:

 

    Public Sub dialogShown_cb()
        Try
        
            '---- Enter your callback code here -----
            group.Show = toggle0.Value
 
        Catch ex As Exception
        
            '---- Enter your exception handling code here -----
            theUI.NXMessageBox.Show("Block Styler", NXMessageBox.DialogType.Error, ex.ToString)
        End Try
    End Sub

Re: toggle disables group

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom
Thanks for the response.

i'm going to test this and let you know if it works

Ruud van den Brand
Pre-sales NX CAD
cards PLM Solutions