Cancel
Showing results for 
Search instead for 
Did you mean: 

turn off disable measurement feature

Creator
Creator

Hello,

 

I'm using NX 9.0.3.4. Each time I measure something in a design, a measuement feature is added to the feature tree. So I end up with frequently cleaning up the feature tree from all these useless measurement features. Is there a way to stop NX from creating measurement features?

 

Kind regards, Edwin

 

 

9 REPLIES

Re: turn off disable measurement feature

Valued Contributor
Valued Contributor

I am not sure if this works in NX9, it does work in NX10.

You can make a favorite which isn't associative. In the dialog options: choose "show collapsed groups", in associative measure and checking: toggle off associative. Save this as a favorite which you can use instead of the default simple measurement. . You can do this for all simple measurement options.

W10 NX11.0.1 almost NX12.0.0.27

Re: turn off disable measurement feature

Creator
Creator

I not only dislike seeing it. I do not want it to be there. It is byond me why anybody would like to see a simple measurement popping up in the feature tree. So I want it to be completely switched off. And most likely such can be done in NX...the trick is to find where the setting is hidden

 

Re: turn off disable measurement feature

Honored Contributor
Honored Contributor

In the measure distance command, expand the "associative measure and checking" and turn off the "associative" option; take a measurement (anything) and press the OK button. Assuming that you have "dialog memory" enabled (the default), it will remember your preference the next time you use the command.

Re: turn off disable measurement feature

Valued Contributor
Valued Contributor

The associative option is only remembered with the normal measurement commands. It won't be stored for the simple measurement commands.

 

W10 NX11.0.1 almost NX12.0.0.27

Re: turn off disable measurement feature

Creator
Creator

So....what it boiles down to is that you can switch this 'feature create' mode off for the high level measure command. But for the simple measure commands this disabling is impossible, as it will switch itself on uncontrollably. Good programming Siemens!

Re: turn off disable measurement feature

Esteemed Contributor
Esteemed Contributor

Have you already checked the customer defaults?

I would search for measure or associative.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.0, FBM, MRL 3.1.4 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 10.1
Development: VB.NET, Tcl/Tk    Testing: NX12.0

How to Get the Most from Your Signature in the Community

Re: turn off disable measurement feature

Creator
Creator

Hi Stefan,

 

Unfortunately, nothing found there...

Simple measurement simply always turns on associative. So either turn off associative each time it is used, or remove the feature after measurement is done. Or end the command with 'cancel' instead of 'ok'....but there is no way to change the default

Re: turn off disable measurement feature

Esteemed Contributor
Esteemed Contributor

If you file an IR at GTAC I will be happy to get us added to it Smiley Wink

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.0, FBM, MRL 3.1.4 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 10.1
Development: VB.NET, Tcl/Tk    Testing: NX12.0

How to Get the Most from Your Signature in the Community

Re: turn off disable measurement feature

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

there's enough IRs already logged for this one (see below), but there is an ER to attach to (1947098):

 

  • Symptom
  • ---------------
    The 'simple measurement' commands (Simple Distance/Diameter/Angle/Length) 
    create an unwanted 'measurement' feature in the Part Navigator by default.
    Unchecking the 'Associative Measure and Checking - Associative' option in the
    command dialog is not remembered between each use of the 'simple' measurement
    command.
    
    (Note: This is the as-designed behavior for the 'simple measurement' commands.
    They have no dialog memory to ensure they have a simple and consistent
    behaviour each time they are used.)
  • Hardware/Software Configuration
  • Family: NX
    Application: DESIGN
    Function: INFO_ANALYSIS
    Subfunction: MEASURE_DIST
    Release: V8.5 and later releases
  • Solution
  • A workaround to the issue is to select 'Cancel' on the 'Simple Distance' 
    dialog (rather than 'OK' or 'Apply') to prevent the distance measurement from 
    being created in the Part Navigator.
    
    An alternative approach is to create a ‘Favorite’ of the ‘Simple Distance’
    command, with the ‘Associative’ option deselected. This can be added to the
    ribbon bar to replace the out-of-the-box command.
    
    The procedure to do this is outlined below;
    
    1. Start NX and select the ‘Analysis’ tab to display the ribbon bar.
    
    2. Select the ‘Simple Distance’ command and then the ‘Dialog Options’ menu (the
    cog in the top left-hand corner of the command dialog), select ‘Show Collapsed
    Groups’.
    
    3. Expand the ‘Associative Measure and Checking’ group and uncheck the
    ‘Associative’ option.
    
    4. Collapse the ‘Associative Measure and Checking’ group and select ‘Hide
    Collapsed Groups’ from the ‘Dialog Options’ menu.
    
    5. Again select ‘Dialog Options’ and choose  ‘Save Favorite As...’
    
    6. Enter a name for the new command, for example ‘New Simple Distance’, select
    ‘OK’. ‘Cancel’ the measure command dialog.
    
    7. Select the ‘Simple Distance’ command icon with the right-hand mouse button
    and choose ‘Customize’.
    
    8. On the ‘Commands’ tab, select ‘New Item’ from the ‘Categories’ list and then
    select ‘New User Command’ from the ‘Items’ list. Drag and drop the ‘New User
    Command’ option next to ‘Simple Distance’ command on the ribbon bar.
    (The ‘Customize’ dialog should remain open.)
    
    9. Select the ‘User Command’ icon on the ribbon bar with the right-hand mouse
    button and choose ‘Edit Action’. Select ‘Favorite’ from the ‘Type’ pull-down
    and select ‘New Simple Distance’ from the ‘Favorite’ list. Select ‘OK’.
    
    10. Select the ‘Simple Distance’ command with the right-hand mouse button and
    choose ‘Copy Button Icon’.
    
    11. Select the ‘New Simple Distance’ icon with the right-hand mouse button and
    choose ‘Paste Button Icon’;
    
    12. Select the ‘Simple Distance’ command with the right-hand mouse button and
    choose ‘Delete’. ‘Close’ the ‘Customize ‘ dialog.
    
    13. Use the ‘New Simple Distance’ icon to measure without creating a
    measurement feature in the Part Navigator
    
    Repeat the process above to create ‘favorites’ for the other ‘simple measure’
    commands, such as ‘Simple Angle’.
    These user interface changes are stored for use in subsequent NX sessions.
    
    For further information please refer to the NX documentation articles entitled;
    ‘Save a command dialog box layout as a favorite’
    ‘Add a favorite command to the Ribbon bar’
  • Reference
  • Note: There is an enhancement request (ER 1947098) to add a customer default to
    control the setting on the 'Associative' option within the 'simple 
    measurement' commands.
Anthony Galante, Senior Support Engineer
PhoenxPLM
24 versions of NX installed: NX4 to NX12, plus TC11.2