Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Re: 有关于钣金模块的折弯扣除表的使用

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello @王远兮 

The format of your table looks correct to me.

 

You have set your bend radius to 0.5 for all thicknesses so this should work fine.  Make sure your feature dialogs (flange, etc.) have the Bend Radius set to global factor so this value is read and all features will have the same bend radius.

 

If you would like to attached your standards file or send direct to me I can check and test it for you.

 

One further comment: Do you really want a fixed bend radius for all thicknesses?  I'd suggest having 0.5 for all will not be possible in reality - the material will fracture.  A bend radius of at least the material thickness is advised with Steel.

 

Many thanks,

 

Dave

Re: 有关于钣金模块的折弯扣除表的使用

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @王远兮 

I would like to make a correction to a previous post regarding the Bend deducution table.

The table takes three inputs and generates a single output.  My prevous post identified some areas incorrectly.  Please see the image below for the correct description:

2019-08-14 15_28_22-Clipboard.png

NX Sheet Metal
NX Sheet Metal

This group is dedicated to the discussion of Sheet Metal in NX.

Members (116)