@ dave_walker, cannot remove all internal bodies to make it ready for "convert to sheetmetal" . some bodies are removed, not all. Alert comes "This operation cannot make multiple bodies. this holes are required, because this cut-out holes provides as "edge rip" flat pattern
Internal bodies came from holes
At some stages of remove, alert comes, cannot remove rest faces
shell command, trying to remove internal bodies
Holes created from extrude> substruct operation
Hello @Omar_bd,
It is not clear to me what you are trying to achieve here?
For convert to sheet metal to work, the input body should already look like a sheet metal part. Maybe a different techique is required for you?
Can you provide a model that represents the desired shape (ignore rips for now) so I can better understand your design intent?
Thanks,
Dave
Desired shape (conical bend involved): required to be flattable
to make it flattable, Edge rip is required along red line. at top side, rip is done by extrude(substruction) in solid model
Hi @Omar_bd,
This shape may be a little too complex for a simple Convert to Sheet Metal operation. if you can't even create the shell in modeling then it is an unlikely candidate.
Try converting just parts of the design and do not define the rips before conversion, do it during.
Other options are Sheet Metal from Solid or the Forming Flattening tool in Modeling (image below is my effort)
Finally, if you can't model it directly in Sheet Metal then it is unlikely that Convert to Sheet Metal will process it - after all, that is the purpose.
Best of luck,
Dave
@ dave_walker, cannot remove all internal bodies to make it ready for "convert to sheetmetal" . some bodies are removed, not all. Alert comes "This operation cannot make multiple bodies. this holes are required, because this cut-out holes provides as "edge rip" flat pattern
Internal bodies came from holes
At some stages of remove, alert comes, cannot remove rest faces
shell command, trying to remove internal bodies
Holes created from extrude> substruct operation
This group is dedicated to the discussion of Sheet Metal in NX.
User | Rank |
---|---|
Siemens Honored Contributor | |
Enthusiast | |
Solution Partner Creator | |
Theorist | |
Creator | |
Solution Partner Creator | |
Dreamer | |
Creator | |
Solution Partner Creator | |
Solution Partner Legend |