Cancel
Showing results for 
Search instead for 
Did you mean: 

Corner like contour flange

Phenom
Phenom

Hi,

I would like to obtain the result like the image with the red arrow. I try to use the 'Bend taper' command, without success.

2018-11-22_12-35-23.jpg

Thank you...

Using NX1859
RuleDesigner PDM

2 REPLIES 2

Re: Corner like contour flange

Valued Contributor
Valued Contributor

2018-11-22_131902.png

try a Three Bend Corner

(did it in NX 12, see the part is NX 11)

 

Highlighted

Re: Corner like contour flange

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

See below

 

stream.gif

Corner like contour flange

Phenom
Phenom

Hi,

I would like to obtain the result like the image with the red arrow. I try to use the 'Bend taper' command, without success.

2018-11-22_12-35-23.jpg

Thank you...

Using NX1859
RuleDesigner PDM

NX Sheet Metal
NX Sheet Metal

This group is dedicated to the discussion of Sheet Metal in NX.

Members (100)