Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Help on sheet metal design

Phenom
Phenom

Hi,

I want to replicate a standard modeling into a sheet metal approach. Attached the file.

Body (1) is the imported, after I tried with Convert to Sheet Metal Wizard but the result I don't like.

After I start to try starting to zero, but when I want to incline the flange (6) with Bend Taper, I'm not able to obtain a good result. Suggestions ?

Thank you...

Using NX11 and NX1847
RuleDesigner PDM

2 REPLIES

Re: Help on sheet metal design

Siemens Phenom Siemens Phenom
Siemens Phenom

When Convert to Sheet Metal doesn't quite give the result you are after, try Sheet Metal From Solid.

Have a look at the attached part and see if it works for you.  This part was created in NX11.0.1.

 

Dave

Re: Help on sheet metal design

Siemens Phenom Siemens Phenom
Siemens Phenom
Actually, try Convert to Sheet Metal and then run Cleanup after.
Highlighted

Help on sheet metal design

Phenom
Phenom

Hi,

I want to replicate a standard modeling into a sheet metal approach. Attached the file.

Body (1) is the imported, after I tried with Convert to Sheet Metal Wizard but the result I don't like.

After I start to try starting to zero, but when I want to incline the flange (6) with Bend Taper, I'm not able to obtain a good result. Suggestions ?

Thank you...

Using NX11 and NX1847
RuleDesigner PDM

NX Sheet Metal
NX Sheet Metal

This group is dedicated to the discussion of Sheet Metal in NX.

Members (91)