Cancel
Showing results for 
Search instead for 
Did you mean: 

How to convert to sheet metal for this part

Phenom
Phenom

Hi,

I tried to convert to sheet metal this part without a good result. Someone have time to use his sheetmetal experience to suggest me the correct workflow ?

Thank you...

Using NX1867
RuleDesigner PDM

4 REPLIES 4

Re: How to convert to sheet metal for this part

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @cubalibre00,

 

The part looks like it converted but the design cannot be manufactured due to overlapping faces.

2018-05-08 08_46_33-Siemens NX - Sheet Metal.jpg

Some things to check on your conversion though.

  • When edges are ripped, check that you have clearance between faces (advise at least 0.2 here to be sure)
  • 2018-05-08 08_48_49-Clipboard.jpg
Highlighted

Re: How to convert to sheet metal for this part

Phenom
Phenom

@cubalibre00

 

You have a conflicting overlap of flanges.

So I quickly did some extra cutouts to free up some material:

But of course it's up to you to decide how it should be done in reality...

2018-05-08_01.gif2018-05-08_02.gif2018-05-08_03.gif

I also added some blends at these corners just to be sure the weren't touching anymore:

 

2018-05-08_11.gif

 

hopefully this gets you started Smiley Wink

Huysmans Metalen n.v.
2x NX1867 Mach Designer
on Win10 64bit
NX Beta Tester with focus on Sheet Metal
Command Finder is your friend

Re: How to convert to sheet metal for this part

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

Hi @cubalibre00,

Using additional edge rips (add existing Convert to SM and remove small edges selected for ripping) with section can help to update Convert to SM with a better geometry. Bend Taper can be used to remove interference in flattened state. Attached part has been updated with this way.

 

CCG4Z0592-0005_solutions.JPG

 

Regards

 

Regards,
Amol

Re: How to convert to sheet metal for this part

Phenom
Phenom

Hi @Amol_Badgujar,

your suggestion has give me the final solution that I attach.

 

Thank you...

Using NX1867
RuleDesigner PDM

How to convert to sheet metal for this part

Phenom
Phenom

Hi,

I tried to convert to sheet metal this part without a good result. Someone have time to use his sheetmetal experience to suggest me the correct workflow ?

Thank you...

Using NX1867
RuleDesigner PDM

NX Sheet Metal
NX Sheet Metal

This group is dedicated to the discussion of Sheet Metal in NX.

Members (112)