Cancel
Showing results for 
Search instead for 
Did you mean: 

Ring with a profile

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Hello everyone!

Is it possible to flatten using the NX sheet metal?

I suspect it is not and I need to emulate flattening using the regular NX modeling tools, but maybe?

8 REPLIES

Re: Ring with a profile

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @Scaffold

Yes you can.  You just need to do it in two stages, see attached.

 

Dave

Highlighted

Re: Ring with a profile

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

What a one big piece of an elegant solution! Thanks a lot! Man Happy

Re: Ring with a profile

Gears Phenom Gears Phenom
Gears Phenom

Can I join the elegancy contest? Smiley Happy

 

2019-01-11_40.gifNX12 Part Navigator; Ring with Contour Flanges2019-01-11_39.gifNX12; Ring With Flanges

Huysmans Metalen n.v.
2x NX 12.0.2.9 Mach Designer
on Win10 64bit
NX Beta Tester with focus on Sheet Metal
Command Finder is your friend

Re: Ring with a profile

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Equally great! Thank you! Man Happy

Re: Ring with a profile

Enthusiast
Enthusiast

@Frank: very efficient. I like it.

 

I wonder if its possible, to do it with only 1 secondary contour flange.

Re: Ring with a profile

Gears Phenom Gears Phenom
Gears Phenom

@HolgerSwat_BSH

 

I didn't try but I made a quick reflection on that;

If your goal is to have the least features, it might work. But that would mean that the secondary contour flange would need to start on a cone.

A cone means a Lofted Flange; and creating that Lofted Flange means two sketches...

And with the Lofted Flange you might have a very hard time to get the exact position of the bend between Lofted Flange and Contour Flange.

Huysmans Metalen n.v.
2x NX 12.0.2.9 Mach Designer
on Win10 64bit
NX Beta Tester with focus on Sheet Metal
Command Finder is your friend

Re: Ring with a profile

Enthusiast
Enthusiast

@frank_nx: I think, you're right. every attempt to save one secondary contour flange makes more features or a lot more complicated features nesessary.

Re: Ring with a profile

Gears Phenom Gears Phenom
Gears Phenom

 

@HolgerSwat_BSH

Anyway you made me curious and I did a quick try;

It doesn't work:

2019-01-11_41.gifNX12 Attempt for secondary CF on edge of Lofted Flange

 

 

EDIT:

@Dave_Walker

This reminds for the Lofted Flange;

This should work in a future improved Lofted Flange Smiley Wink

Huysmans Metalen n.v.
2x NX 12.0.2.9 Mach Designer
on Win10 64bit
NX Beta Tester with focus on Sheet Metal
Command Finder is your friend

Ring with a profile

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Hello everyone!

Is it possible to flatten using the NX sheet metal?

I suspect it is not and I need to emulate flattening using the regular NX modeling tools, but maybe?

NX Sheet Metal
NX Sheet Metal

This group is dedicated to the discussion of Sheet Metal in NX.

Members (91)