Cancel
Showing results for 
Search instead for 
Did you mean: 

NX 11 Bead Command Error

Experimenter
Experimenter

Hello, I'm getting an error in BEAD command. When I pick the curve on the desired face the following message pops up: "Section must lie on a face of the body. Edit section" I've created curve with both SKETCH command and SKETCH SECTION option in BEAD window.

 

Would you please let me know what I'm doing wrong?

2 REPLIES 2

Re: NX 11 Bead Command Error

Phenom
Phenom

I am assuming that you are using the Sheet Metal Bead command.

 

To use it, the part must be a sheet metal model.

 

You will get that error message if you try to create a bead on a regular solid model.

 

Highlighted

Re: NX 11 Bead Command Error

Experimenter
Experimenter
Thank you very much!! It is goog to know. I have created the bead manually
from modelling interface.