Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Object creation dependent on an input

Experimenter
Experimenter

Hello, 

 

I have a problem with my MCD project. I control the simulation with a PLC. Via an object source, new objects are created in a magazine, with a frequency of 4 seconds. These are pushed onto a conveyor belt via a slider. Via the PLC I can stop the slider and the conveyor belt. Unfortunately, objects will still be created, which then fall into each other.

 

Is there a possibility to create the objects depending on a shared memory variable? E.g. that I will set a "4" by the variable, so that every 4 seconds an object is created, or with "0" no object at all.

 

Unable to play video. Please try again later.
(view in My Videos)