Cancel
Showing results for 
Search instead for 
Did you mean: 

1 in 10 quality check

Pioneer
Pioneer

Hi, I want to have a quality check for an OptionalGage. I want the RobotC to take one in every ten entities. Right now I have it set up so that it chooses a random number and if that number is in the .00-.10 range the RobotC takes it. This is 10% as opposed to one in ten and I was wondering if there was any way to simulate that. I've attached a picture below. Thanks in advance!

3 REPLIES 3

Re: 1 in 10 quality check

Phenom
Phenom

Did you for example have a look at the discrete Empirical (dEmp) or uniform (z_uniform) distribution if that's you

you mean by "simulate that"

Re: 1 in 10 quality check

Pioneer
Pioneer
Sorry for the confusion I moved this from a different forum and forgot to post the pictures. I just uploaded them. What are dEmp and z_uniform could you elaborate? Thanks

Re: 1 in 10 quality check

Phenom
Phenom

@dEmp and z_uniform

 

These are defined distributions.

 

For details please refer to the plant Simulation help

 

Looking at your posted screenshots - you are already using the z_uniform distribution

Unbenannt.PNG