Cancel
Showing results for 
Search instead for 
Did you mean: 

1 method 2 behaviors

Pioneer
Pioneer

Hi guys,

 

short:

in my model i have a method which search in a specific table for some parts.

In the first try it works how i should but in the next pass nothing happens.

 

now a larger description:

i have different stations which need different parts. these parts are shipped via transporters to the stations. At that stations they are unloaded depends on which part is needed (searching in a table). In the first pass the vehicle is unloaded how it should but when the other transporter comes nothing happens.

 

Better have a look at my model for understanding.

 

I thought about this problem nearly 2 hours but i can't explain it to me. Hope you guys have an idea.

 

Thanks in advance

 

Carsten

3 REPLIES 3

Re: 1 method 2 behaviors

Pioneer
Pioneer

especially at station 5. But i think that the same problem will happen at station 6, 10 and 12 again because there are the methods the same

Re: 1 method 2 behaviors

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi Carsten,

 

your method E_M5 looks for the MU "Hauptteil_C" but none of your carriers have such a part.

Therefore assembly M5 is never getting the part it is waiting for.

Regards,

Ralf
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.

Re: 1 method 2 behaviors

Pioneer
Pioneer

Hi Ralf,

OHHH MY GOD :-OOO

you're so right.... i was so fixed to the method code that i didn't recognize this litte error... must be a copy & paste fault in my "Teile"-table.

Now that's very embarrassing..

 

Thank you very much!

 

Regards

Carsten