Cancel
Showing results for 
Search instead for 
Did you mean: 

3D Hospital Model - Information Needed

Hello Community,

 

I want to create a 3D model for a hospital using Plant Simulation; therefore I need have a 3D model of: e.g. Nurse, Patient, Doctor, Room, Bed, etc... I wonder where I can get this information and is it availble in Siemens libraries?

 

Also, I wonder if I can integrate another tool with Tecnomatix such as Siemens NX or Solid Edge to import the 3D model.

 

Mohamed Elshal

3 REPLIES

Re: 3D Hospital Model - Information Needed

Siemens Phenom Siemens Phenom
Siemens Phenom
Hello Mohamed,
I'm not aware of a library which contains these 3D models. But both NX and SolidEdge can export JT which you then can import into Plant Simulation.
Regards,

Ralf
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.

Re: 3D Hospital Model - Information Needed

Is there a specific file format for the 3D objects to be imported to Tecnomatix?

Re: 3D Hospital Model - Information Needed

Siemens Phenom Siemens Phenom
Siemens Phenom
Yes, Plant Simulation uses the JT (.jt) file format.
Regards,

Ralf
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.