Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

3D - part & new mu both visible

Builder
Builder

Hi all,

 

I've a problem with my assembly station in my 3D model. (see image attached)

During the process, a part of the assembly AND the new mu are both visible. The new mu is not only visible on exit, or on start of the process such as in 2D....

How to only see one of the parts and no both ? How to set differently the mus position of the new mu and the parts ?

 

Many thanks !

2 REPLIES 2

Re: 3D - part & new mu both visible

Siemens Phenom Siemens Phenom
Siemens Phenom

If you create an exit control in your assembly's predecessor that is rear-triggered with the following code:

 

is

do

    @._3D.VisibleGraphics := makeArray();

end;

 

then it should work.

Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution

Re: 3D - part & new mu both visible

Builder
Builder

Yeah, it works !

 

Thanks a lot Smiley Happy