Cancel
Showing results for 
Search instead for 
Did you mean: 

A problem about Recovery time

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hello Expert,

I have assigned a recovery time in the SingleProc object ,but it doesn't work.

Is it means that, when a part enter the SingleProc object, recovery time and proc time consume at the same time?

Thanks very much!

2 REPLIES 2

Re: A problem about Recovery time

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

You have to select the point in time, when the recovery-time calculation is started ("recovery time starts").

 

"Is it means that, when a part enter the SingleProc object, recovery time and proc time consume at the same time?"

 

Yes, if you select "When part enters"; then you need to define a recovery time greater than the processing time to take into account additional machining times (cleaning, clamping, loading, unloading...). The other options starts after processing or after exiting the part.

 

In the statistics you find the recovery time as waiting time.

 

 

Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net

Re: A problem about Recovery time

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor
Hello Steffen_B,
Thanks for your help, I have learned a lot from your many answers.
And, Happy Christmas!