Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

AGV implementation

Creator
Creator

Hi Everybody,

i am using Plantsimulation V 10.1.7, i have seen in the manual that there is a Folder OF AGVs but when i cant find it.

 

i dont know if there is allready a methods to simulate AGV or not?

 

thanxagv.png

4 REPLIES 4

Re: AGV implementation

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

You need to include the AGV library into your model:

File - Manage Class Library --> Tab Libraries

But it is available only until version 10 of Plant Simulation.

 

If you have also a V. 10 installation on your computer, then you can load the library using the context menu of the classlibrary in 10.1 --> Save/Load --> Load object. You will find the AGV library in the installation of Plant Simulation 10 Folder: Libraries - Standard - Free - Transport --> AGVS.lib

 

Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net

Re: AGV implementation

Creator
Creator

Hi Steffen_B
in the Folder that you mentioned i just have : Cranes.lib, fuzzy.lib, and kanban.lib

 

 

 

Re: AGV implementation

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

your version is 10.1

AGV is available until 10 only.

Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net

Re: AGV implementation

Creator
Creator

ah ok.

Thank you very much Steffan