Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Access violation problem.

Creator
Creator

Hello everyone,

 

For an unknown reason, the model stops and receive the following message. Does anyone understand the meaning?

 

Thank you

Shimon

1 REPLY 1

Re: Access violation problem.

Siemens Phenom Siemens Phenom
Siemens Phenom

The application crashed because of a bug in the software. I would recommend that you install the service pack 12.0.2 and check if this solves the problem. Otherwise, if you have a maintenance contract, I would recommend that you open an IR (you can do this via 'File > Help > Log an Incident with Technical Support' from the main menu).

_________________________________________________________________
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.