Cancel
Showing results for 
Search instead for 
Did you mean: 

Add length-oriented object to frame via SimTalk

Valued Contributor
Valued Contributor

Hi all,

 

I was wondering if it's possible to add a length-oriented objected into a frame via SimTalk. Looked on Learing Advantage, Forum, and Help material, but couldn't find an answer.

 

Many thanks.

4 REPLIES 4

Re: Add length-oriented object to frame via SimTalk

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
have a look on createObject, this also works with length oriented objects
Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net

Re: Add length-oriented object to frame via SimTalk

Valued Contributor
Valued Contributor

Oh, I couldn't find anything about this on PS help files. But thanks for the reply, I managed to do what I was trying.

 

There is no information regarding this method on PS help files. However, I've found this thread that giver some further light into the CreateObject method, if anyone is interested: https://community.plm.automation.siemens.com/t5/Plant-Simulation-Forum/How-to-insert-objects-by-Simt...

Re: Add length-oriented object to frame via SimTalk

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
look also here

https://community.plm.automation.siemens.com/t5/Plant-Simulation-Forum/Regarding-Segment-table/m-p/4...
Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net

Re: Add length-oriented object to frame via SimTalk

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello,

 

for this case you can also look up the method "derive" in the manual, as "createObject" is a deprecated method that was replaced by "derive".

Kind regards,

Igor
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution