Cancel
Showing results for 
Search instead for 
Did you mean: 

An error in creating the new icon of MUs

Experimenter
Experimenter

0.png

How to fix it? Thanks.

1 REPLY 1

Re: An error in creating the new icon of MUs

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello Brian,

 

you are using a rather old version of Plant Simulation. For this version the most current maintenance pack is 15 (9.0.15). So if possible you should upgrade to the latest maintenance pack.

 

This version is also no longer under support. So it would also make sense to update to a newer version.

Regards,

Ralf
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.