Cancel
Showing results for 
Search instead for 
Did you mean: 

Animation gets locked when source produces MU

Valued Contributor
Valued Contributor

If I have a source producing Multiple MU in the middle of the run when the source starts producing MU the animation pauses as the events occur in same time. But even if I use interval at source the MU are produced at a same instance of the time. 

 

You can see in the below attached model that I have used 10 seconds interval to produce at the source but still the MU get produced at a particular instance of time only.

 

What may have gone wrong?

 

1 REPLY 1
Highlighted

Re: Animation gets locked when source produces MU

Siemens Phenom Siemens Phenom
Siemens Phenom

In the source you have checked 'Generate as batch'. Therefore all the MUs are created at once.

Regards,

Ralf
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.