06-12-2018 04:35 AM
Hello community,
I want to implement a frame "test" (see attached screenshot) in my simulation model. The frame "test" includes a conveyor. In the end, my goal is to show the MUs also on the symbol of the frame "test". In other word, I want to animate the frame "test" without showing the object "conveyor".
Does anybody have an idea, if there is an option to animate only MUs on a frame symbol?
Thanks in advance !
Solved! Go to Solution.
06-12-2018 04:44 AM
Steffen Bangsow freelance simulation specialist web: www.bangsow.eu mail: steffen@bangsow.net | ![]() |
06-12-2018 04:55 AM
That was easy! Thank you