Cancel
Showing results for 
Search instead for 
Did you mean: 

Application crashes when copying the method object

Experimenter
Experimenter

Hi everybody,

 

when i try to copy a method object from one network to another or to the same network, the application always crashes.

What could be the reason?

 

Thanks in advance

4 REPLIES

Betreff: Application crashes when copying the method object

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello F_KR,

 

which version of Plant Simulation did you use?

 

Regards
GG

------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution

Betreff: Application crashes when copying the method object

Experimenter
Experimenter

Hello GG,

 

I use version 14

Betreff: Application crashes when copying the method object

Gears Phenom Gears Phenom
Gears Phenom

I encountered crashes sometimes when copying a large amount of objects at once, but not with a single object. Can you post the method source-code, or better yet the method-object, or best: your whole model? Then we could test it Smiley Happy

Alex

___________________________________________________________
Alex Dilg, Consultant at SimPlan AG (www.SimPlan.de)
This post was good and/or helpful to you? Please provide some Kudos, thank you!

Betreff: Application crashes when copying the method object

Experimenter
Experimenter

I don't think that the problem appends on the method source-code or on the method-object, because it appears in fewer method-objects, also with no source-code in it.

I think it is a problem in the Network or the class where the method-object is placed in my library, because the problem only appears in a specific subnetwork in a network of a userdefined library.

Unfortunately I'm not allowed to post my Model.