Cancel
Showing results for 
Search instead for 
Did you mean: 

Assembly ChangeOver

Pioneer
Pioneer

Hello,

 

I have a question,  say I have two customers sharing an assembly line and i want to model a changeover (when the line is down to switch from one customer to another) what is the best way to do this? I was thinking I could add it into the build plan of the schedule. I was also thinking maybe using Lockout? Any suggestions?

 

Thank you in advance!

 

Kbohara14

1 REPLY 1

Re: Assembly ChangeOver

Valued Contributor
Valued Contributor

Hi

 

You can set the set-up time of the entrance workstation. And on the tab set-up, you can define which kind of changeover you relly need.

 

Best regard!

 

Tao Yifei