Cancel
Showing results for 
Search instead for 
Did you mean: 

Assembly from 2 lines

Experimenter
Experimenter

Hello,

 

Probably this is already asked. But I have searched an answer but I couldn't find.

 

I have 2 lines. On each line are produced 40 pieces.  This 40 pieces from each line will be assembled at once together. 

How can I do this? Every time there must be assembled 40 pieces of line 1 and 40 pieces of line 2. This should also result in 40 final products. 

I would be very thankful for any help. 

1 REPLY 1

Betreff: Assembly from 2 lines

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello Izlop,

 

you can use the Assembly object. Set the Assembly table to 'Predecessor' and define Predecessor 2 Number 1 in the table which can be opened using the Open button.

 

Hope this helps.

Regards

GG

Regards
GG

------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution