Cancel
Showing results for 
Search instead for 
Did you mean: 

Assembly on container that is located on container

Pioneer
Pioneer

Hello,

 

I know the title does make that much sense but I would like to know how you tacke this chalange.

 

I have an part that contains many assembly. And I have a base part, that contains 10 shafts and then on each of those shafts I would like to assemble a part (gear).

Is this posbile to do without DismentleStation?

 

Thanks and regards

4 REPLIES

Re: Assembly on container that is located on container

Honored Contributor
Honored Contributor
do you want to "load" the gear to the shaft or do you just consume the right number of gears?
Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net

Re: Assembly on container that is located on container

Genius
Genius

Hello HugoZupan,

 

yes, it is possible. 

- Create a user defined table (lets say 'available_shafts') in the base part (Container) and update the path / name / type of the 10 shafts available in it.

- When base part along with 10 shafts move to respective assembly station, check the 'available_shafts' table and track each shaft whether it is occupied or not (or specific shaft). if not occupied, then assemble a gear to the shaft.

 

Thanks & Best Regards,

Abhilash Sridhar.

Thanks & Best Regards,
Abhilash Sridhar
Mercedes Benz R&D India, Daimler AG

Re: Assembly on container that is located on container

Pioneer
Pioneer

Yes I would like to load the gear to the shaft

Re: Assembly on container that is located on container

Pioneer
Pioneer

Here is an example what i mean