Hello
I have the following model where product A and product B are pulled by customer order, it works well, however I need to expand it and include product configuration or modulariaiton, specifically, I need the following :
In Stage1 :
- When demand part A arrives in BKQueue 1, Part A is assembled by mixing Raw material 1 and 2 and 3
- When demand part B arrives in BKQueue1, Part B is assembled by mixing Raw material 1 and 3.
- Currently there is only two sources, and have Mu. for part A and B which I believe should change to three sources raw material 1, raw material 2 and 3.
- In the end, the report should still present Product A and Product B. Would someone help me do this modificaiton on my model ? please feel free to modify on the model itself, that would help me see it and expand it even further. thanks alot !
Farouq