Cancel
Showing results for 
Search instead for 
Did you mean: 

Assembly station on 2 containers

As can be seen in the file attached i've a problem with the assembly station; basically i have 2 types of container, the highlighted "fibbia" and "telaio_12".

The process is this; 12 pcs of containers "fibbia" (predecessor 2) needs to stored in 1 pcs of "telaio_12" (predecessor 1) with the assembly station.

"fibbia" needs to be a container because later on it'll be assembled with other types of MUs.

Honestly i didn't understand if it's possibile to assembly a container with another or not but in the help and in the forum i haven't found any answer.

If i start a simulation everything stops when the buffer before the assembly station are full.

Do you have any suggestion? 

Thanks.

3 REPLIES 3

Re: Assembly station on 2 containers

i've found a way and the model seems to work as can be seen in the image attached.

However i don't know how to assemble 12 pcs of "fibbia" in 1 pcs of "telaio_12".

thanks.

Re: Assembly station on 2 containers

Phenom
Phenom
Change "number" from 1 to 12
Highlighted

Re: Assembly station on 2 containers

i've done in a different way; i've made main mu form predecessor: 2 and in the table 12 of predecessor 1 and it's working.
Thanks for your help.