Cancel
Showing results for 
Search instead for 
Did you mean: 

Assign a shift calendar

Pioneer
Pioneer

Hello everyone!

 

I have an issue with the use of the Shiftcalendar.

I have a plant with several machines and all machines have a different Shiftcalendar. All these shift calendar are located in the same frame (different from the plant).

Every beginning of week, I assign a new calendar to the machines :

.Models.Plant.Machine1.ShiftCalendarObject := .Models.Frame.Calendar_machine1;

When I am running my models, I do not see any Pausing time on my machines.

 

Do someone knows why this do not take into account the shift calendars?

 

Thanks in advance for your help.

Regards,

 

Geraldine

2 REPLIES 2

Re: Assign a shift calendar

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi Geraldine,

 

I don't see a problem with what you're doing.

 

Can you post a model which shows the behavior you see?

 

Regards,

Ralf

Regards,

Ralf
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.

Re: Assign a shift calendar

Pioneer
Pioneer

Hi Ralf,

 

Thanks for your answer.

Meantime I have find an alternative (if the shift calendars are in a related frame, it is working).

 

Regards,

Geraldine