Cancel
Showing results for 
Search instead for 
Did you mean: 

Assigning custom worker creation table (with additional services)

Creator
Creator

Hi,

 

I'm new with PlantSim and SimTalk (using v 13 educational 30-day trial) and struggeling to simulate different scenarios for the worker pool.

 

Goal:

I want to test two scenarios for workload and idle times: a) with 8 workers and b) with 9 workers. In each case, each worker is responsible for a set of machine (which differs between the cases), while one is a floater who can work anywhere.

 

What I've tried:

 

- In order to assign only one worker to a set of stations, I've defined one additional service for each station and an alternative 'floater service' for all of them

 

- Manually entering workers and services via the WorkerPool Creation table. Problem: I can add new lines, but not new colums - they seem to be limited to 4 (not counting the ones already labeled by PlantSim). Is that due to using a trial license? -> Just found out it's necessary to save & close both the table and worker pool and reopen them, new colums will be created automatically. Clicking 'apply' isn't enough...

 

- Creating two table objects with the specifications, then using an init-Method and setCreationTable to assign one to the worker pool, but directly referring to a table doesn't work.

 

Is there a way to assign custom worker tables directly (either via a general init or the experiment manager) to the WorkerPool or would that require to loop through every argument?

 

Thanks in advance for your help!

 

 

 

 

4 REPLIES

Re: Assigning custom worker creation table (with additional services)

Honored Contributor
Honored Contributor

look into this example (Small Example collection) in Plant Simulation:

www.png

Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net

Re: Assigning custom worker creation table (with additional services)

Creator
Creator

Hi Steffen,

 

thanks for your answer. I have looked into the example and managed to adjust the experiment (adding the same worker type in the table, assigning him a higher efficiency and creating some sample cases with different worker numbers). Crucial was finding the "Extras-More Options-Use Configuration Method" - I had been trying to solve setting the table via dragging an init-Method into the model, which didn't work.

 

But when trying to recreate the example, it's still not working. Could you give me a hint on what's missing?

 

 

Re: Assigning custom worker creation table (with additional services)

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi Peritectic,

 

the Experimentmanager needs a terminating simulation.

If you insert an end time into the Eventcontroller then you can start the experiment study.

 

Regards,

Peter

Re: Assigning custom worker creation table (with additional services)

Creator
Creator

Hi Peter,

 

Thank you very much, now it's finally working! Smiley Happy

 

Regards,

Peritectic