Cancel
Showing results for 
Search instead for 
Did you mean: 

Assigning failure parametres by method from a centralized table

Builder
Builder

Dear all!

 

I have the following situation, where I am unable to realize this in a method:

 

FailuresbyMethod.jpg

For a station, I would like to assign certain parameters for a failure by a method. Therefore a table is prepared containing the name, the pointer to the object, the particular failure profile and in the subtable, the parameters for start, stop, interarrival time interval and duration. The availability / MTTR approach is not sufficient.

 

I want to use more than one failure profile being parameterised by the table lines. Therefore the easy way to use the easy approach (FailureDuration etc.) is no option.

 

How can I use the "setParam" command to alter the parametres providing the appropriate path to the attribute from the table of failures as described in the online help? When I try to concatenate the different cells in a row and converting the result to an object, I am failing because of addressing an attribute.

 

Thx!

10 REPLIES 10

Re: Assigning failure parametres by method from a centralized table

Phenom
Phenom
Why are you using your own formatted table and not the

table provided by object.failures.getTable(table) ?

This table would be easier for handling the failure settings though object.failures.setTable(table) .

Re: Assigning failure parametres by method from a centralized table

Builder
Builder

Why is it not possible to answer a single question, but immediately questioning the way someone else is working with PlantSimulation outside of the Siemens playgrounds?

 

Among a certain amount of other reasons, I found the table not intuitive at all. When providing the approproiate data using "setParam" I was expecting, that a PlantSimulation internal check may point out, if there is a mistake left in the parameterisation. Just concatenating the parameters to a string without any possibility to validate is by far not what I regard as user friendly and effective.

Re: Assigning failure parametres by method from a centralized table

Phenom
Phenom

Apparently because you're way didn't work ...

 

I tested the setparam and it didn't work in the "failure" constellation

 

so I suggested the settable solution as the best solution.

 

It is not clear to me , why it is more effective for you

to write parameters into a table and then try to use - in a further step

setparam with concatenated table parameters- to set the failure profiles.

 

settable does this in one step

 

Re: Assigning failure parametres by method from a centralized table

Builder
Builder

So this means, the corresponding description in the helpfile, which I was trying out for the last two days is just rubbish?

 

setParam-Help.jpg

 

I know better ways to waste my time.

Re: Assigning failure parametres by method from a centralized table

Phenom
Phenom

There seems to have been a missunderstanding were I / how I tested the setparam (failure level) and

 

where you expected then to work ( attribute level).

 

In any case I checked the "help" screen shots and they work. s. attachment

 

 

Unbenannt.png

Re: Assigning failure parametres by method from a centralized table

Siemens Phenom Siemens Phenom
Siemens Phenom

SetParam works exactly as documented in the online help. I do not know what you are doing wrong, because you never showed us your SimTalk code. Maybe you just entered the path to the failure profile instead of the full path to one of the 4 times of the profile (Start, Stop, Interval, Duration).

You could use setTypeAndAttr instead of setParam. This method always expects 2 strings. The first string is the distribution type, and the second string is for the distribution parameters.

SingleProc.Failures.Failure1.Interval.setTypeAndAttr("Negexp", "45:00")
SingleProc.Failures.Failure1.Duration.setTypeAndAttr("Erlang", "5:00, 3:30")

 

_________________________________________________________________
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.

Re: Assigning failure parametres by method from a centralized table

Builder
Builder

Ok, so now it works.

 

Anyway this brings me back to my original question posted at the beginning: How can I use this or the setParam command if I have everything related to including the path stored in a parametre table (see initial posting).

 

I wasn't able to properly concatenate the particular command line as provided in the example above using the information from the table cells and couldn't find any hint on this problem in the online help. The recent replies above aren't helping me in any way.

 

 

Re: Assigning failure parametres by method from a centralized table

Siemens Phenom Siemens Phenom
Siemens Phenom

If you have the entire path to the failure profile in a string, the only solution I can think of is to use the execute statement:

var path : string := "SingleProc.Failures.Failure1"
var type : string := "Uniform"
var para : string := "1, 5:00"

execute(to_str(path, ".Duration.setTypeAndAttr(\"", type, "\", \"", para, "\")"))
_________________________________________________________________
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.

Re: Assigning failure parametres by method from a centralized table

Builder
Builder

Thanks, that seems what I was looking for. Gonna check it in near future.

 

I guess, it's SimTalk 2.0, but it shouldn't be a problem to apply it to SimTalk 1.0.