Cancel
Showing results for 
Search instead for 
Did you mean: 

At 11 objects i exceed the maximum objects for the student version..?!

Experimenter
Experimenter

I get this message when I only have added 11 objects. The student version should let me work with 80 objets.. What should I do to get it right?

 

 I have to do this assignment for school soon so I would appreciate a quick anser. Thanks!

problem.jpg

5 REPLIES 5

Re: At 11 objects i exceed the maximum objects for the student version..?!

Siemens Phenom Siemens Phenom
Siemens Phenom

Maybe you have loaded some libraries with a high object count. You can select "Manage Class Library" in the toolbar. Please deselect all libraries you don't need.

 

If the problem is still there you can send us the model and we will have a look at it:

plantsimulation.studentlicense.plm@siemens.com

Regards,

Ralf
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.

Re: At 11 objects i exceed the maximum objects for the student version..?!

Experimenter
Experimenter
Thank you very much, it seems to work now!

Re: At 11 objects i exceed the maximum objects for the student version..?!

Siemens Phenom Siemens Phenom
Siemens Phenom

You can also create a method with the following code:

 

is
do
	print NumOfLimitedObjects;
end;

 

It will print the number of objects to see how close to the limit you are.

Regards, Vladimir.

Re: At 11 objects I exceed the maximum objects for the student version..?!

Experimenter
Experimenter

Where do I write that? It did stop me again now when I have 20 objects, after remowing some features.

Re: At 11 objects I exceed the maximum objects for the student version..?!

Siemens Phenom Siemens Phenom
Siemens Phenom

You have to insert a method object and copy the SimTalk code into the method.

The number of objects is then printed into the console window when you run the method.

 

But this just gives you the same information as you can see in the top of your class library window.

 

If you want us to look into it just send us the model to the e-mail address mentioned above.

Regards,

Ralf
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.