Cancel
Showing results for 
Search instead for 
Did you mean: 

Attribute for Dwell time on buffer

Creator
Creator
Hello, I try to built a simply buffer with a dwell time depending of the attribute of MUs. What is the easiest way to do that, because I can write the attribute in the dwell time (it only accepts a constant). If I put a method in entrance to update the proctime, it change the dewll time for all the MUs inside the buffer and not only the current MU... Thanks,
1 REPLY 1

Re: Attribute for Dwell time on buffer

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Hi Jer_N,

 

I checked and it seems you are right, but it is not that surprising. I think the underlying issue is that the MUs are not allowed to overtake each other.

 

You can try to use a ParallelProc instead. There you can give each MU a unique time. I recommend to change the Resource type on the Statistics tab to Storage.

 

Regards,

Gert Nomden


Gert Nomden
Senior Consultant | Tecnomatix Product Manager
cardsplmsolutions.com