Cancel
Showing results for 
Search instead for 
Did you mean: 

Automatic routing with destination lists

Pioneer
Pioneer

Good morning, I have been studiying with Mr Bangsow book and examples and I have a doubt in one of them, it is called automatic routing with destination lists and I don't know why the simulation stops after 4 minutes and it doesn't continues forever.

 

Thank you 

2 REPLIES 2

Re: Automatic routing with destination lists

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
the exitcontrol of track1 has to be rear, not front (if you use a front exit control, you need to move the MU e.g. @.move).

A other way is to use a sensor with the setting "only if destination", so you can use the routing function of Plant Simulation also for not connected objects and you need only the programming to move the parts to the destination.
Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net

Re: Automatic routing with destination lists

Pioneer
Pioneer
Thank you Mr Bangsow