Cancel
Showing results for 
Search instead for 
Did you mean: 

Average of Chart Input

Experimenter
Experimenter

Hi there.

 

This is my first post so I apologize if I do something I should not.

 

I just started working with Tecnomatix Student version and I was wondering if it is possible to create an average of the Resource information displayed in a chart of 3 different Stations (Single Proc).

 

I attached an image of the chart displaying the info of 3 different stations: M1, M2 and M3.

My final goal is to get an average of the 3 values and just display 1 column.

 

Would help me to figure this one out?

 

Thanks a lot in advance.

 

tecnomatix.PNG

 

 

 

 

2 REPLIES 2

Betreff: Average of Chart Input

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello AlvaresFlores,

 

just double click the chart to open its dialog. There you will find the button 'TableFile' on tab 'Data'.

Press the button to see a table with the values which will be displayed.

Here you can enter 'M1.statWorkingPortion+M2.statWorkingPortion+M3.statWorkingPortion/3' to get the average value.

 

Hope this will help.

 

Regards

 

GG

 

 

Regards
GG

------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution

Highlighted

Betreff: Average of Chart Input

Experimenter
Experimenter

Thanks a lot Smiley Happy

 

I do still have one question. Is it possible to do it with cell coordinates. For example instead of 'M1.statWorkingPortion+M2.statWorkingPortion+M3.statWorkingPortion/3' I can use (1,2)+(1,3)+(1,4)/3