Cancel
Showing results for 
Search instead for 
Did you mean: 

Backward Movement in Line Object

Creator
Creator

Hello,

 

I am using Technomatix Plant Simulation version 10.1.2. In my model, I have a requirement of moving the MUs from the end to start of the line in the reverse direction. But, the problem is that the cycle works only 1 time. I have attached an example model.

 

Please help me how can I make the motion uniterrupted.

 

Thanks

2 REPLIES

Re: Backward Movement in Line Object

Phenom
Phenom

change your method to (s.below),

delete it from the entrance- and insert it in the exit-ctrl

is
do
	waituntil line1.empty prio 1;
	@.Move(Line1, 10);
end;

 

 

Re: Backward Movement in Line Object

Creator
Creator

Thank you for the solution Sir!!!Smiley Very Happy