Cancel
Showing results for 
Search instead for 
Did you mean: 

Backwards animation

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

Hello everyone,

 

I was wondering if it is possible to play self animation backwards through simtalk.

 

Thanks in advance

5 REPLIES

Re: Backwards animation

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello learner,

 

the method "schedule" has an optional parameter of type boolean.

When you call schedule with true the animation is played backwards.

Regards,

Ralf
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.

Re: Backwards animation

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

Hello Ralf,

 

Thanks for your answer. Now my models is more smooth. :-)

Re: Backwards animation

Valued Contributor
Valued Contributor
Hallo Ralf,

I have the same query in my model.
I tried to use the following two codes.
Ani.Path1.Schedule(true);
Ani.Path1.schedule= true;

However, it says the method does not require a Parameter. Could you please provide an example method call? Thank you so much for your time.

Regards

Re: Backwards animation

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello Simpulse,

 

the optional parameter for the method schedule was added in version 12.1.

 

So if you have an older version, it's not yet available.

Regards,

Ralf
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.

Re: Backwards animation

Valued Contributor
Valued Contributor
Hello Ralf,

Thank you for the quick Reply. That is exactly my Problem. I will update my Version then.

Regards