Cancel
Showing results for 
Search instead for 
Did you mean: 

Bar and Line chart in One Graph in Plant Simulation

Experimenter
Experimenter

Hello Mr. Tobel,

 

I want to make a chart as mentioned below in Plant Simulation.

Is this possible ?

 

if Yes, how?

 

Thanks in advance

 

testDemandCapacitychart- Plantsim..PNGDemand Capasiity Graph

2 REPLIES 2
Highlighted

Re: Bar and Line chart in One Graph in Plant Simulation

Siemens Phenom Siemens Phenom
Siemens Phenom

The only way to achieve this is to use annotations for the lines.

I created a small example model to demonstrate it.

_________________________________________________________________
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.

Re: Bar and Line chart in One Graph in Plant Simulation

Experimenter
Experimenter

Thank you very much!!!!